LTE TDD

DL-FRC Wizard Config (Advanced TDD Downlink)

For Waveform Playback (ARB) capability.

Configures Advanced TDD Downlink carrier with FRC settings. The DL-FRC Wizard Config button is shown when an Advanced Downlink carrier is added.

SCPI Command

[:SOURce]:RADio:LTETdd:WAVeform[:ARB]:CCARrier<n>:TDLink:CONFig:FRC <string>

SCPI Example

RADio:LTETdd:WAVeform:CCARrier1:TDLink:CONFig:FRC "FrcType: RRECeiver, SystemBandwidth: BW10, UeCategory: CAT1L1"

Notes

Set only (Immediate Action).

The string is a comma-separated list of key:value pairs for all DL FRC wizard settings.

State Saved

No

Min

N/A

Max

N/A

Preset

Refer to the element definition of the data part below.

Range

Refer to the element definition of the data part below.

Initial S/W Revision

A.20.01

Element definition of the data part. The preset value is basically the same as the default value of each setting definition.

Settings

Symbols in the data part

Values in the data part

Preset values

FRC Type

FrcTypeSetting

RRECeiver|MILC3to5|MILC1|MILC2|QPSKR13|QAM16R12|QAM64R34|SPRBedge|TAP2|TAP4|FRCFDD

RRECeiver

System Bandwidth

SystemBandwidthSetting

BW1_4|BW3|BW5|BW10|BW15|BW20

BW5

RB Offset

RbOffset

0-99 (integer)

N/A

FRC QPSK R1-3

FrcQpskR1_3

R2|R4

N/A

FRC QAM16 R1-2

FrcQam16R1_2

R3

R3

FRC QAM64 R3-4

FrcQam64R3_4

R5|R6|R7|R8|R9

N/A

FRC Single PRB

FrcSinglePrb

R0|R1T10|R1T20

N/A

FRC Two Antenna

FrcTwoAntenna

R10|R11|R30

N/A

FRC Four Antenna

FrcFourAntenna

R12|R13|R14

N/A

FRC FDD Sub Type

FrcFddSubType

R15|R16|R17

N/A

UE Category

UeCategorySetting 

CAT1L1|CAT2L2|CAT3L2|CAT4L2|CAT5L4|CAT6L2|CAT6L4|CAT7L2|CAT7L4|CAT8L8|CAT9L2|CAT9L4|CAT10L2|CAT10L4|CAT11L2|CAT11L4|...|CAT14L8|...|CAT21L4

CAT14L8

Carrier Advanced TDD Downlink ARB

Welcome to LTE TDD